1. Home
Comunicado de Imprensa

Siemens extends Veloce hardware-assisted verification support of EPGM Ethernet to 1.6 Tbps

18 de dezembro de 2024
Plano, Texas, USA

Siemens Digital Industries Software announced today an extension of its Veloce™ hardware-assisted verification platform to support 1.6 Tbps Ethernet. As a core component of the Siemens software/hardware and system validation platform, Veloce delivers complete virtual models to support Ethernet Packet Generator and Monitor (EPGM) Ethernet port speeds up to 1.6 Tbps. This enables full performance, pre-silicon verification for complex networking designs targeting data center, cloud, HPC and AI workloads. 

The Veloce hardware-assisted verification platform now supports the evolving standard of IEEE 802.3dj for port speeds of 1.6 Tbps based on 200G per lane and also supports 200G/400G/800G performance based on the 200G per lane technology standard. 

“These interfaces enable customers to scale up large networking configurations for skyrocketing bandwidth demand,” said Jean-Marie Brunet, vice president and general manager, Hardware-Assisted Verification, Siemens Digital Industries Software. “The Veloce low latency, high bandwidth co-model channel provides a complete, high-performance pre-silicon environment so customers can easily run complex system-level scenarios for maximum functional and performance verification of Ethernet devices.”  

Availability 

The Veloce portfolio of supported DUT interfaces for 200G, 400G, 800G and 1.6T Ethernet (based on 200G/lane technology) is available now. To learn more about how Siemens is enabling the semiconductor and electronic systems industry to deliver to market the world’s most advanced SoCs and systems, visit: https://eda.sw.siemens.com/en-US/ic/hav/ 

A Siemens Digital Industries Software ajuda empresas de todos os portes em sua transformação digital usando software, hardware e serviços da plataforma Siemens Xcelerator. O software da Siemens e o gêmeo digital abrangente permitem que as empresas otimizem seus processos de projeto, engenharia e manufatura para transformar as ideias de hoje em produtos sustentáveis do futuro. De chips a sistemas inteiros, de produtos a processos, para todos os setores. Siemens Digital Industries Software– Accelerating transformation.

Obs.: A lista de marcas comerciais relevantes da Siemens pode ser visualizada aqui. As outras marcas comerciais pertencem aos seus respectivos proprietários.

Contato para jornalistas

Siemens Digital Industries Software PR Team

Email: press.software.sisw@siemens.com