1. Home
Informacja prasowa

Siemens works with Arm and AWS to bring PAVE360 to the cloud and unlocks next generation automotive innovation

14 listopada 2023
Plano, Texas, USA

Siemens works with Arm and AWS to bring PAVE360 to the cloud and unlocks next generation automotive innovation
  • Siemens Digital Industries Software, together with Arm and AWS, delivers breakthrough PAVE360 digital twin solution on AWS’s cloud services to help accelerate next-generation software defined vehicle (SDV) innovation with virtual car in the cloud
  • Developers can now access Arm automotive technology on AWS as part of PAVE360 digital twin solution to help customers speed development of automotive systems

Siemens Digital Industries Software today announced that its PAVE360-based solution for automotive digital twin is now available on AWS. Expanding on the strong partnership between Siemens and AWS, PAVE360 helps foster innovation in the automotive industry through hardware and software parallel development, “shifting-left" the design phase of SDV. With a parallel approach, developers can compress the design cycle time and accelerate time to market. In addition, Siemens has collaborated with Arm to help enable developers to access Arm®-based technology running on Siemens’ PAVE360 Digital Twin solution via AWS cloud services.

Automakers are now able to develop software and evaluate key Arm-based system and software components earlier in their IP selection and design cycles, without the burden of conventional on-premises software, simply by accessing the PAVE360 solution available on AWS. This not only helps address the technology and commercial challenges ahead but also helps empower developers to gain a competitive advantage by shifting left hardware and software development, with unprecedented simulation speeds, enabling them to meet shrinking time-to-market requirements. By using AWS technology, developers can experience near real-time simulation speeds which are significantly faster than conventional on-premises modeling and simulation infrastructures.

“The automotive industry is facing disruption from multiple directions, but the greatest potential for growth and new revenue streams is the adoption of the Software Defined Vehicle (SDV),” said Mike Ellow, Executive Vice President, EDA Global Sales, Services and Customer Support, Siemens Digital Industries Software. “The hyper-competitive SDV industry is under immense pressure to quickly react to consumer expectations for new features all while being pushed to move towards shorter software development cycles. This is driving the adoption of the “shift-left” methodology for parallel hardware and software co-development and the move toward the holistic digital twin. Delivering PAVE360 on Arm-based AWS cloud services helps enable organizational efficiencies that are simply not available through today’s traditional development methods.”

Siemens’ PAVE360, deployed on AWS includes IP from Arm that is built for automotive-specific workloads, functional system software, real-world stimulus and algorithm development tools such as Simcenter™ Prescan from Siemens, and class-leading mixed-fidelity EDA modeling and simulation engines. PAVE360 seamlessly integrates all these sources to provide not only a virtual car on an engineer’s desk but also a virtual car in the cloud that is more integrated and secure, dramatically reducing resources and costs for manufacturers. This helps to eliminate the need for costly IT upgrades to support high-speed simulation and can free up automotive engineers to focus on making more meaningful improvements.

"The software defined vehicle is survival for the automotive industry, requiring new technologies and methodologies for faster and more agile development,” said Dipti Vachani, Senior Vice President and General Manager, Automotive Line of Business, Arm. “The innovative Siemens’ PAVE360 solution is helping to accelerate the automotive system development required to address the increasingly demanding consumer expectations. Together with Siemens and AWS, we are enabling a breadth of use cases on the Arm automotive platform across the entire supply chain, from IP evaluation to fleet management.” 

“The proliferation of digital twin methodologies throughout the automotive industry uses the compute capabilities and world-class infrastructure of AWS,” said Wendy Bauer, Vice President of Automotive and Manufacturing, AWS. “With PAVE360 mapping accurate embedded environments to optimal AWS instances while using Arm automotive enhanced IP, OEMs and suppliers are enabling software defined vehicle solutions and methodologies that were previously impractical.”

PAVE360 via AWS is available now to selected customers. To learn more about how Siemens is working with AWS and Arm to bring the power of PAVE360 to the cloud and how automotive developers can shift-left with faster, centralized virtual design of next generation software defined vehicles, visit: https://eda.sw.siemens.com/en-US/pave360/

Siemens Digital Industries Software pomaga organizacjom każdej wielkości w cyfrowej transformacji przy użyciu oprogramowania, sprzętu i usług z platformy biznesowej Siemens Xcelerator. Oprogramowanie firmy Siemens i kompleksowy cyfrowy bliźniak umożliwiają firmom optymalizację procesów projektowania, inżynierii i produkcji, aby przekształcić dzisiejsze pomysły w zrównoważone produkty przyszłości. Od chipów po całe systemy, od produktu po proces, we wszystkich branżach. Siemens Digital Industries Software– Accelerating transformation.

Siemens Digital Industries (DI) jest liderem innowacji w zakresie automatyzacji i cyfryzacji. Ściśle współpracując z partnerami i klientami, DI napędza cyfrową transformację w przemyśle procesowym i dyskretnym. Dzięki portfolio Digital Enterprise, DI zapewnia firmom każdej wielkości kompleksowy zestaw produktów, rozwiązań i usług do integracji i cyfryzacji całego łańcucha wartości. Zoptymalizowane pod kątem specyficznych potrzeb każdej branży, unikalne portfolio DI wspiera klientów w osiągnięciu większej wydajności i elastyczności. DI stale dodaje innowacje do swojego portfolio, aby zintegrować najnowocześniejsze technologie przyszłości. Siemens Digital Industries ma swoją globalną siedzibę w Norymberdze w Niemczech i zatrudnia około 76 000 pracowników na całym świecie.

Siemens AG (Berlin i Monachium) jest firmą technologiczną skupiającą się na przemyśle, infrastrukturze, transporcie i opiece zdrowotnej. Od bardziej zasobooszczędnych fabryk, odpornych na ryzyka łańcuchów dostaw, inteligentnych budynków i sieci, po czystszy i bardziej komfortowy transport oraz zaawansowaną opiekę zdrowotną - firma tworzy technologie z myślą o tworzeniu realnej wartości dla klientów. Łącząc świat rzeczywisty i cyfrowy, Siemens umożliwia swoim klientom przekształcanie ich branż i rynków, pomagając im zmieniać codzienność miliardów ludzi. Siemens posiada również większościowy udział w notowanej na giełdzie spółce Siemens Healthineers, wiodącym na świecie dostawcy technologii medycznych kształtującym przyszłość opieki zdrowotnej. Ponadto Siemens posiada mniejszościowy udział w Siemens Energy, globalnym liderze w dziedzinie przesyłu i wytwarzania energii elektrycznej.

W roku podatkowym 2022, który zakończył się 30 września 2022 roku, Grupa Siemens osiągnęła przychód w wysokości 72,0 mld euro i dochód netto w wysokości 4,4 mld euro. Na dzień 30 września 2022 roku, firma zatrudniała na całym świecie około 311 000 pracowników. Więcej informacji można znaleźć na stronie www.siemens.com.

Uwaga: Lista właściwych znaków handlowych Grupy Siemens jest dostępna tutaj. Pozostałe znaki towarowe należą do ich odpowiednich właścicieli.

Kontakt dla prasy

Zespół ds. PR spółki Siemens Digital Industries Software
press.software.sisw@siemens.com