1. Home
Informacja prasowa

Hamamatsu Photonics adopts Siemens‘ mPower for optical semiconductor design

14 grudnia 2022
Plano, Texas, USA

Siemens Digital Industries Software announces today that Hamamatsu Photonics K.K. (Hamamatsu Photonics), a leading provider of optical semiconductor devices, has adopted Siemens' award-winning mPower™ digital software for the power integrity analysis of its next generation of optical semiconductor devices.

By pursuing further advancement of photoelectric conversion technology to discover the true nature of light, Hamamatsu Photonics delivers high-sensitivity, fast-response and high-performance optical semiconductor devices. The company provides a wide range of products such as photodiodes, photo ICs, image sensors, infrared detection devices and LED offerings – all of which support multiple wavelength ranges (e.g., infrared, visible, ultraviolet, x-ray, high-energy). The products are widely used in many applications, including the scientific measurement, medical and automotive markets.

“Power integrity analysis is a critical technology for us, because our optical IC products need to achieve extremely high performance and reliability in order to meet stringent functionality requirements,” said Masaaki Matsubara, manager for the second design group, Design Center, Solid State Division for Hamamatsu Photonics. “We believe Siemens’ mPower digital software is our best option for improving IC performance and reliability. Our designers use the mPower solution to analyze their designs at early stages of development, and the software definitely helps to optimize the power source design faster.”

Introduced last year, Siemens’ mPower solution aids customers to more quickly and accurately perform sign-off analysis of the power, electromigration and IR-drop performance of integrated circuits (ICs), helping them to confirm that their as-implemented design will meet performance and reliability targets when manufactured.

Siemens’ mPower digital software provides power integrity analysis with high accuracy through fast and efficient distributed processing. Featuring an intuitive graphical user interface for optimal ease-of-use, the solution supports analysis across the IC design process, from initial concept design to design sign-off, helping users to create better designs with no compromise in quality or speed. For optimal reliability and IC traceability, the mPower solution also integrates seamlessly with Siemens’ Calibre® RVE software, which is part of its industry-leading Calibre® platform for IC physical verification.

“As image sensors grow in size and complexity, it becomes both harder and more critical to verify the power integrity of these very large designs,” said Joe Davis, senior director for Interfaces and EM/IR Product Management for Siemens EDA. “Hammamatsu Photonics quickly determined that the mPower solution provides the capacity, performance, and integration that they need in order to bring high performance, high resolution sensors to the market and we look forward to working with them as they bring more advanced designs to the market.”

Siemens Digital Industries Software pomaga organizacjom każdej wielkości w cyfrowej transformacji przy użyciu oprogramowania, sprzętu i usług z platformy biznesowej Siemens Xcelerator. Oprogramowanie firmy Siemens i kompleksowy cyfrowy bliźniak umożliwiają firmom optymalizację procesów projektowania, inżynierii i produkcji, aby przekształcić dzisiejsze pomysły w zrównoważone produkty przyszłości. Od chipów po całe systemy, od produktu po proces, we wszystkich branżach. Siemens Digital Industries Software - where today meets tomorrow.

Uwaga: Lista właściwych znaków handlowych Grupy Siemens jest dostępna tutaj. Pozostałe znaki towarowe należą do ich odpowiednich właścicieli.

Kontakt dla prasy

Zespół ds. PR spółki Siemens Digital Industries Software
press.software.sisw@siemens.com