1. Home
Informacja prasowa

Siemens delivers a major leap toward mainstream 3D-IC adoption with new Calibre 3DThermal

24 czerwca 2024
Plano, Texas, USA

  • Calibre 3DThermal delivers complete chip and package-inward thermal analysis software for 3D-ICs, addressing critical design and verification challenges from early-stage chip and 3D assembly exploration to design signoff
  • New offering integrates with Siemens’ advanced design tools to provide a robust platform that captures and analyzes thermal data throughout the design process

Siemens Digital Industries Software today introduced Calibre® 3DThermal, innovative software for thermal analysis, verification and debugging in 3D integrated circuits (3D-ICs). Calibre 3DThermal enables chip designers to rapidly model, visualize and mitigate thermal effects in their designs from early-stage chip and package-inward exploration through to design signoff by incorporating elements of Siemens’ Calibre verification software and Calibre® 3DSTACK software along with the company’s Simcenter™ Flotherm™ software solver engine. Calibre 3DThermal provides the outputs necessary for thermal impacts to be considered in electrical simulations. Moreover, Calibre 3DThermal can both consume as input boundary conditions as well as provide output to Simcenter Flotherm – enabling true IC to system thermal modeling from IC to package to board to system level.

Calibre 3DThermal was developed to address challenges of 3D-IC architectures where controlling heat dissipation is a key requirement. It offers fast, accurate, powerful and comprehensive approaches to identifying and rapidly addressing complex thermal issues. Calibre 3DThermal provides the flexibility to start initial feasibility analysis with minimal inputs and can later perform more detailed analyses considering metalization details and their impact on thermal considerations as more detailed information becomes available. This progressive approach enables designers to refine their analysis and apply fixes such as floorplanning changes and adding stacked vias or TSVs to avoid thermal hotspots and/or dissipate heat more effectively. This iterative process continues until the final assembly is complete, significantly reducing the risk of performance, reliability and manufacturing issues at final tape-out.

Delivering thermal analysis at this advanced level requires a complete understanding of the 3D-IC assembly. Waiting until the assembly is complete to identify and correct errors can severely disrupt design schedules, but Calibre 3DThermal mitigates this risk through automation and integration, allowing designers to iterate thermal analysis at whichever design stage they are working on.

Calibre 3DThermal embeds a custom version of Siemens’ accurate, industry-trusted Simcenter Flotherm software solver engine to create precise chiplet-level thermal models for static or dynamic simulation of full 3DIC assemblies. Debugging is streamlined through the traditional Calibre RVE software results viewer, which is already integrated across a wide range of IC design tools. The integration of these powerful tools results in an efficient thermal analysis solution tailored to the specific needs of 3DIC designers.

Like all Calibre products, Calibre 3DThermal integrates seamlessly with a range of industry-leading design tools from both third parties, as well as with Siemens’ software including the newly announced Innovator3D IC™ software. In all design flows, Calibre 3DThermal captures and analyzes thermal data across the entire design lifecycle.

“Calibre 3DThermal represents a significant advancement in 3D-IC design and verification, providing designers with the capabilities they need to address thermal challenges early in the design process,” said Michael Buehler-Garcia, vice president, Calibre Product Management, Siemens Digital Industries Software. “By integrating thermal analysis directly into all stages of the IC design flow, we’re enabling our customers to create more reliable, high-performance 3DICs with greater confidence and efficiency.”

Collaboration with UMC

In a collaborative effort, Siemens has joined forces with United Microelectronics Corporation (UMC) to deploy an innovative thermal analysis flow for UMC customers powered by Calibre 3DThermal. This cutting-edge software is tailored specifically for UMC’s wafer-on-wafer and 3D-IC technologies and has been validated and is planned for availability to UMC’s global clientele soon.

“As the semiconductor industry grapples with escalating thermal challenges, particularly in the realm of heat dissipation and thermal gradients within advanced 3D-IC technologies, UMC remains committed to providing effective solutions,” said Osbert Cheng, vice president of device technology development & design support at UMC. “Through our collaboration with Siemens and the implementation of Calibre 3Dthermal, we will be able to offer our customers a comprehensive thermal analysis capability, enabling them to address critical thermal concerns and optimize their designs for enhanced performance and reliability.”

To learn more about Calibre 3DThermal visit https://eda.sw.siemens.com/en-US/ic/calibre-design/3dthermal/

Siemens Digital Industries Software pomaga organizacjom każdej wielkości w cyfrowej transformacji przy użyciu oprogramowania, sprzętu i usług z platformy biznesowej Siemens Xcelerator. Oprogramowanie firmy Siemens i kompleksowy cyfrowy bliźniak umożliwiają firmom optymalizację procesów projektowania, inżynierii i produkcji, aby przekształcić dzisiejsze pomysły w zrównoważone produkty przyszłości. Od chipów po całe systemy, od produktu po proces, we wszystkich branżach. Siemens Digital Industries Software– Accelerating transformation.

Siemens Digital Industries (DI) jest liderem innowacji w zakresie automatyzacji i cyfryzacji. Ściśle współpracując z partnerami i klientami, DI napędza cyfrową transformację w przemyśle procesowym i dyskretnym. Dzięki portfolio Digital Enterprise, DI zapewnia firmom każdej wielkości kompleksowy zestaw produktów, rozwiązań i usług do integracji i cyfryzacji całego łańcucha wartości. Zoptymalizowane pod kątem specyficznych potrzeb każdej branży, unikalne portfolio DI wspiera klientów w osiągnięciu większej wydajności i elastyczności. DI stale dodaje innowacje do swojego portfolio, aby zintegrować najnowocześniejsze technologie przyszłości. Siemens Digital Industries ma swoją globalną siedzibę w Norymberdze w Niemczech i zatrudnia około 72 000 pracowników na całym świecie.

Siemens AG (Berlin i Monachium) jest firmą technologiczną skupiającą się na przemyśle, infrastrukturze, transporcie i opiece zdrowotnej. Od bardziej zasobooszczędnych fabryk, odpornych na ryzyka łańcuchów dostaw, inteligentnych budynków i sieci, po czystszy i bardziej komfortowy transport oraz zaawansowaną opiekę zdrowotną - firma tworzy technologie z myślą o tworzeniu realnej wartości dla klientów. Łącząc świat rzeczywisty i cyfrowy, Siemens umożliwia swoim klientom przekształcanie ich branż i rynków, pomagając im zmieniać codzienność miliardów ludzi. Siemens posiada również większościowy udział w notowanej na giełdzie spółce Siemens Healthineers, wiodącym na świecie dostawcy technologii medycznych kształtującym przyszłość opieki zdrowotnej.

W roku podatkowym 2023, który zakończył się 30 września 2023 roku, Grupa Siemens osiągnęła przychód w wysokości 77,8 mld euro i dochód netto w wysokości 8,5 mld euro. Na dzień 30 września 2023 roku, firma zatrudniała na całym świecie około 320 000 pracowników. Więcej informacji można znaleźć na stronie www.siemens.com.

Uwaga: Lista właściwych znaków handlowych Grupy Siemens jest dostępna tutaj. Pozostałe znaki towarowe należą do ich odpowiednich właścicieli.

Kontakt dla prasy

Zespół ds. PR spółki Siemens Digital Industries Software
press.software.sisw@siemens.com