보도 자료

Siemens extends Veloce hardware-assisted verification and validation with new Innexis shift-left software

2024년 11월 7일
Plano, Texas, USA

  • Innexis delivers a set of products and capabilities to address demand for shift-left software development in the IC development process
  • With more demanding software workloads, it is critical to facilitate the development and execution of realistic workloads early in the design phase to shorten overall development time and identify hardware and software defects earlier

Siemens Digital Industries Software announced today the Innexis product suite, a complement to its industry leading Veloce™ hardware-assisted verification and validation system.

Building on the success and rapid adoption of Veloce, Siemens’ Innexis product suite delivers a set of capabilities to address customer demand for shift-left software in the early phases of IC development. These products include a hardware/software development flow from virtual to hybrid to full RTL, an architecture native virtual platform for early high-speed software development and a simulation backplane that enables the development of digital twins in Siemens’ PAVE360™ software for software-defined vehicles and other complex systems.

“The complexity of integrated circuits (IC) is increasing exponentially, designers need more efficient methodologies to meet industry demands. Veloce has seen rapid adoption by industry leaders to help solve this critical bottleneck. The Innexis product suite extends workflow improvements from Veloce to help our customers shift left their IC development and debug cycle,” said Jean-Marie Brunet, vice president and general manager, Hardware-Assisted Verification, Siemens Digital Industries Software. “This enables IC design to begin months before final RTL, all while using a common software workload across the development process.”

Adoption of a shift-left approach for software development and IP verification processes is now mandatory. As chip designs become increasingly complex due to more demanding software workloads, it is critical to enable the development and execution of realistic workloads early in the design phase. A proactive shift-left software approach helps mitigate the risk of identifying issues late in the development cycle.

“The implementation of Innexis in our development process has significantly enhanced software and system validation performance, thereby improving the efficiency of our teams and projects. By enabling heterogeneous component modeling within virtual platforms, it allows us to create realistic high-speed models of System on Chips (SoCs),” said Ari Hautala, Principal System Architect, Nokia Mobile Networks. “Furthermore, the integration of these high-speed virtual platforms with RTL IP on Veloce emulators facilitates superior overall performance while still permitting precise cycle-accurate performance and power analysis on RTL model components. Additionally, Innexis offers exceptional visibility and debuggability for the SoC design, along with the capability to integrate and execute a large number of complex test cases effectively.”

Currently, the Innexis product suite consists of:

Innexis Developer Pro: Innexis Developer Pro software provides a connected development flow from virtual to hybrid to full RTL. This provides a comprehensive environment for accelerating the creation of complex SoC design supporting a wide range of use-cases including seamless hardware-software co-development, co-validation, and pre-silicon cycle accurate analysis and validation. Innexis Developer Pro supports the modelling of complex SoC’s with heterogeneous cores and custom SystemC model components. In addition, it provides the ability to run in both virtual plus RTL hybrid mode for high performance execution, and then at a time of interest switch to full RTL emulation enabling high accuracy analysis of the full SoC when required.

Innexis Architecture Native Acceleration (ANA): Innexis Architecture Native Acceleration software is a cloud- based high-speed virtual platform. By running natively on Arm based servers the software workloads run at much higher speeds than on typical instruction set simulation based virtual platforms. Cloud hosting also provides scalable compute resources and simple browser-based access and tools. Innexis Architecture Native Acceleration can also run on local Arm based servers if preferred. In both cases it enables early software development and testing, and early software defect identification.

Innexis Virtual System Interconnect: Innexis Virtual System Interconnect software facilitates the creation and simulation of comprehensive system level digital twin platforms by seamlessly connecting multi-behavioral virtual and physical subsystems, supporting a variety of communication protocols. Innexis Virtual System Interconnect behavioral models can include Innexis Developer Pro or Innexis Architecture Native Acceleration SoC models, supporting system-level shift-left software development and RTL verification.

To learn more about Siemens’ Innexis product suite and how it addresses the demand for shift-left software development in the integrated circuit development process, visit: www.siemens.com/innexis

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처