1. Home
Comunicato stampa

Arc adopts Siemens Xcelerator to electrify the marine industry

2 giugno 2025
Plano, Texas, USA

Arc uses Siemens Xcelerator to disrupt the recreational boat industry with all-electric, zero emissions propulsion and delight its customers through a combination of seamless software and hardware integration and outstanding industrial design (Image credit: Arc).
  • Marine industry disruptor leverages Siemens’ NX, Teamcenter and Simcenter software to help develop category defining products across recreational and commercial marine industry

Siemens Digital Industries Software announced today that Arc Boat Company (Arc), a startup on a mission to electrify the marine industry, has adopted the Siemens Xcelerator portfolio of industry software to design and manufacture their high-performance, fully electric boats.

Founded in 2021, Arc is a venture-backed startup based in Los Angeles, California. The company designs and manufactures everything for its electric boats in-house, including battery packs, powertrain systems, thermal control systems and software. Arc One, the company’s first product, sold out its initial production run and the next generation, Arc Sport, a 500 horsepower (hp) all-electric wake boat, is taking the wake boat industry by storm.

siemens-xcelerator-arc-newsroom-02-1280x720

The company’s first product, the Arc One was designed, built and delivered in just two years with Siemens Xcelerator and redefined what is possible on the water – with zero-emissions (Image credit: Arc).

The Arc team had experience using Siemens software at other companies, so Siemens Xcelerator was a natural choice to be the company's technology platform. As Ryan Cook, co-founder and chief technology officer (CTO) at Arc explains, “We thought if Siemens Xcelerator is going to be our long-term software, we might as well just start with it so we don't have to migrate later.”

The ability to build complex parameterized models in Siemens’ NX™ software from the Siemens Xcelerator portfolio enables Arc to develop adaptable parametric 3D models that support its rapid iteration design, build, test and redesign process. “There's a lot of parameters involved in hull design – deadrise, beam at chine, keel angle, etc.– so we used NX to parameterize them all. With our fully parametric hull model, we would build one boat, gauge performance, collect data and tweak one or two parameters and then build a second boat based on what we learned,” says Cook. “Fast forward to today and we're even more sophisticated because we know the performance characteristics we want out of the vehicle. With a given center of gravity and the type of shape we want to go with, we can do it in one shot with NX.”

siemens-xcelerator-arc-newsroom-03-1280x720

Designed with Siemens Xcelerator, the Arc Sport delivers the thrill of a high-torque, all-electric wakesurfing boat—with zero emissions (Image credit: Arc).

Arc uses Siemens’ Simcenter™ software to simulate its products – a particular challenge when looking to disrupt an industry that continues to rely on gas-powered propulsion systems and long-established marine engineering principles. Arc’s focus on all-electric propulsion brings new design, engineering and manufacturing challenges, which is why they depend on Siemens’ simulation technologies.

Arc also uses Simcenter software to optimize the centre of gravity, which is challenging due to the heavy battery pack, and to optimize across the composite hull, deck and hard top to remove weight. This lightweighting is critical to achieving required performance. Simcenter software also enables the team to carry out smaller-scale part structural, vibration and thermal analysis work across the entire boat.

Arc added Teamcenter® software for Product lifecycle Management (PLM) during development of its second product, the Arc Sport, to optimize its product and production data management as the complexity of both its product and supply chain increased. Today, the company is expanding its operations in the recreational and wake boating industries and has announced its first steps into the commercial marine industry and expanded line of recreational boats including the Arc Coast, a ‘center console’ all-electric boat that targets fishing and other water activities.

siemens-xcelerator-arc-newsroom-05-1280x720

Arc’s goal is to bring the power of software to the marine industry and use industrial design to elevate the customer experience via a simple, beautiful helm, designed with Siemens Xcelerator (Image credit: Arc).

Arc is opening research and development facility at the port of Los Angeles and has begun to build out the charging infrastructure needed to support the ports of Los Angeles and Long Beach’s goal to move to zero emission equipment by 2030. It is also collaborating with Portland, Oregon, shipyard, Diversified Marine, to retrofit a 26-foot-long tugboat for high-performance, zero-emission operations.

As Arc seeks to continue to innovate in the marine industry without using fossil fuel power propulsion methods that don’t fit with today’s requirements for cleaner, more sustainable activities, Siemens Xcelerator is at the heart of its product development process.

siemens-xcelerator-arc-newsroom-04-1280x720

Arc cofounders, Mitch Lee (CEO) and Ryan Cook (CTO) are on a mission to electrify the marine industry (Image credit: Arc).

“We're moving very quickly and it's a lot of fun to try and apply some fundamental engineering principles to the marine industry and see if we can come up with something better. Siemens Xcelerator helps us to get there quicker, develop new category defining products that delight our customers and create the electrification revolution we want to see in the marine industry,” concluded Cook.

To learn more about Arc and how it is taking advantage of the Siemens Xcelerator portfolio of industry software to build an all-electric, zero emissions marine industry, visit https://blogs.sw.siemens.com/marine/2025/06/02/electrify-marine-vessels-with-zero-emissions/

Siemens Digital Industries Software aiuta le organizzazioni di tutte le dimensioni ad affrontare la digital transformation utilizzando il software, l’hardware ed i servizi della piattaforma di business Siemens Xcelerator. Il software offerto da Siemens, unitamente alle tecnologie per la realizzazione di completi digital twin, consentono alle aziende di ottimizzare i propri processi di progettazione, di ingegnerizzazione e di produzione, per trasformare le idee di oggi in prodotti sostenibili del futuro. Da singoli chip fino a interi sistemi, dai prodotti ai processi, in tutti i settori. Siemens Digital Industries Software– Accelerating transformation.

Nota: un elenco dei marchi rilevanti di proprietà di Siemens è consultabile qui. Tutti gli altri marchi menzionati appartengono ai rispettivi proprietari.

Contatti per la stampa

Marie Almeida

Tel: (+33) 06 77 19 80 52; E-mail: marie.almeida@siemens.com

Anna Romanelli - ITALMARCO

Tel: (+39) 02 70 10 46 45 – (+39) 347 745 04 09; E-mail: anna@italmarco.com