1. Home
Comunicato stampa

Siemens brings AI copilot, immersive design and integrated fluid and thermal simulation to NX

1 luglio 2025
Plano, Texas, USA

  • Latest updates to NX and NX X brings natural language, AI driven learning with Design Copilot NX
  • Introduces designer-focused, CAD-integrated thermal and fluid simulation based on Simcenter technology and extends model-based design methods into metrology and inspection
  • Delivers immersive product engineering and collaboration capabilities in partnership with Sony

Siemens Digital Industries Software announced today the latest updates to its NX™ and NX™ X software from the Designcenter suite of product engineering software, including immersive engineering for mixed realty design and collaboration, new design for manufacture capabilities, CAD integrated fluid flow simulation and introducing a new AI copilot for design.

siemens-designcenter-nx-summer-2025-newsroom-01-1280x720.jpg

The latest updates to NX and NX X for product engineering include immersive engineering for mixed realty design and collaboration, new for Design for Manufacture capabilities, CAD integrated fluid flow simulation and introduces a new AI Copilot to aid learning.

“Our work to bring together our product engineering solutions under the Designcenter brand is moving at an incredible pace,” said Bob Haubrock, senior vice president, Siemens Digital Industries Software. “The latest updates to NX reaffirm that our commitment to not only introducing new AI-driven copilot capabilities and Characteristics led MBD for downstream quality and manufacturing, but to also explore new areas for innovation in our long established and industry leading product engineering toolset.”

Design Copilot NX

Delivered with the latest update, the new Design Copilot NX leverages Siemens’ robust learning resources and provides an AI-based natural language interface to enable users to accelerate their learning – whether new to the software or experienced users looking to extend their knowledge and explore new capabilities. By leveraging natural language input and querying, the NX copilot capabilities enable users to find answers to technical queries, best practices and documentation quickly and efficiently.

siemens-designcenter-nx-summer-2025-newsroom-02-1280x720

Design Copilot NX provides an AI-based natural language interface to enable users to accelerate their learning – whether new to the software or experienced users looking to extend their knowledge and explore new capabilities.

Immersive engineering

At CES in 2024, Siemens announced its intention to deliver groundbreaking immersive engineering capabilities, in partnership with Sony and its industry leading mixed reality headset. The latest updates to NX have delivered these capabilities across several product introductions.

Alongside the capabilities of NX Immersive Designer which enable designers and engineers to create, view, and edit 3D CAD designs in virtual reality or augmented reality, most recent updates introduce NX Immersive Collaborator - enabling colleagues, partners and other stakeholders to collaborate in the same virtual reality space. Collaborative sessions can be started directly from the NX interface without the need for extensive preparatory work typically associated with VR collaboration and provide a full range of design review tools to measure, assess and annotate individual parts or entire assemblies.

Design for Manufacturing and extending MBD with characteristics

Introduced in the latest updates, the new NX Inspector is groundbreaking, industry first capability that adds model-based characteristics to a digital twin to extend the use of Model-based Design (MBD) to define downstream quality and manufacturing processes. Based on the Digital Metrology Standards Consortium’s Model-Based Characteristics standard, it enables designers and engineers to define manufacturing PMI that can be reused to drive creation of inspection and metrology processes based on real-time, management data through integration with Teamcenter and Teamcenter Quality.

siemens-designcenter-nx-summer-2025-newsroom-03-1280x720

NX Inspector adds model-based characteristics to extend the use of Model-based Design (MBD) to define downstream quality and manufacturing processes, based on the Digital Metrology Standards Consortium’s Model-Based Characteristics standard.

The new Design for Manufacture (DFM) Advisor automates early manufacturability assessments by analyzing part geometry and identifying potential challenges across multiple manufacturing processes (such as drilling, milling, assembly and molding) and providing actionable feedback directly in the interface. Visual reports can be generated and managed in Teamcenter to share with colleagues and partners, while using the insights to drive additional workflows.

Lastly for DFM enhancements the NX Mold Wizard has been extended to not only introduce standard parts that update in real-time with configuration changes, but also now features enhanced cooling channel simulation tools to enable iteration of cooling systems to achieve the best part quality while optimizing cycle time.

siemens-designcenter-nx-summer-2025-newsroom-04-1280x720

NX Mold Wizard has been extended to not only introduce intelligence standard parts that update with configuration changes.

Adding designer focused simulation based on industry proven technology

With the latest updates, Siemens is also introducing NX™ CFD Designer software, a new CAD integrated design simulation tool, powered by technology from Siemens’ Simcenter™ FLOEFD software. CFD Designer enables designers to access fluid flow and thermal capabilities directly within the NX CAD workspace to support simulation-driven decision making. Designed to be easy to use for those without CFD experience, it uses robust automation to tackle complex tasks like fluid volume detection and meshing on the designers’ behalf. It enables designers to quickly evaluate a range of operating scenarios, what-if studies and geometry variations and compare the results. Alongside the new CFD Designer, Siemens has also extended the capabilities of Performance Predictor to enable designers and engineers to run mechanical stress analyses across entire assemblies.

siemens-designcenter-nx-summer-2025-newsroom-05-1280x720

NX CFD Designer software, a new CAD integrated design simulation tool, enabling designers to access fluid flow and thermal simulation capabilities directly within the NX CAD workspace for the first time.

"Through our comprehensive Frost Radar analysis of the mechanical computer-aided design (MCAD) tools within the Product Lifecycle Management (PLM) industry for 2025, Frost & Sullivan has identified Siemens’ NX software as the clear innovation leader. The Siemens MCAD solutions consistently demonstrate groundbreaking advancements, setting new benchmarks for the entire market. Their unwavering commitment to product innovation, coupled with a deep understanding of manufacturers' evolving needs, positions Siemens as the premier partner for companies seeking to harness the full power of MCAD technology to drive their business forward," said Francisco Dell'era, research analyst, Frost & Sullivan.

From Siemens’ Designcenter suite of product engineering software, NX and NX X with cloud-based integrated product lifecycle management, is part of the Siemens Xcelerator portfolio of industry software. To learn more about how Siemens is helping companies of all sizes, from startups to global enterprises, to innovate, watch the NX YouTube premiere or visit https://plm.sw.siemens.com/en-US/nx/cad-online/latest-nx-cad-version/

Siemens Digital Industries Software aiuta le organizzazioni di tutte le dimensioni ad affrontare la digital transformation utilizzando il software, l’hardware ed i servizi della piattaforma di business Siemens Xcelerator. Il software offerto da Siemens, unitamente alle tecnologie per la realizzazione di completi digital twin, consentono alle aziende di ottimizzare i propri processi di progettazione, di ingegnerizzazione e di produzione, per trasformare le idee di oggi in prodotti sostenibili del futuro. Da singoli chip fino a interi sistemi, dai prodotti ai processi, in tutti i settori. Siemens Digital Industries Software– Accelerating transformation.

Nota: un elenco dei marchi rilevanti di proprietà di Siemens è consultabile qui. Tutti gli altri marchi menzionati appartengono ai rispettivi proprietari.

Contatti per la stampa

Marie Almeida

Tel: (+33) 06 77 19 80 52; E-mail: marie.almeida@siemens.com

Anna Romanelli - ITALMARCO

Tel: (+39) 02 70 10 46 45 – (+39) 347 745 04 09; E-mail: anna@italmarco.com