1. Home
Tisková zpráva

Siemens collaborates with sureCore and Semiwise to pioneer quantum computing ready cryogenic semiconductor designs

20. prosince 2023
Plano, Texas, USA

Siemens collaborates with sureCore and Semiwise to pioneer quantum computing ready cryogenic semiconductor designs
  • Collaboration between Siemens, sureCore and Semiwise to develop cryogenic semiconductor designs capable of operating in extreme cold conditions required for quantum computing

Siemens Digital Industries Software announced today its collaboration with sureCore and Semiwise to develop groundbreaking cryogenic CMOS circuits capable of operating at temperatures near absolute zero – a fundamental component of quantum computing systems. The joint effort holds the potential for dramatic advances in both performance and power efficiency for next-generation integrated circuits (IC) targeting quantum computing – considered the leading edge in the high-performance computing (HPC) research and development.

The key to unlocking the potential of quantum computing for HPC and other fast-growing applications lies in the availability of control electronics capable of operating at cryogenic temperatures. Using advanced analog/mixed-signal IC design technology from Siemens, Semiwise has developed cryogenic CMOS circuit designs featuring cryogenic SPICE models as well as SPICE simulator technology that can perform accurate analyses at cryogenic temperatures.

Semiwise is providing this intellectual property (IP), developed using Siemens’ Analog FastSPICE (AFS), to sureCore for the development of sureCore’s revolutionary line of CryoIP, which aims to enable the design of CryoCMOS control chips seen as crucial for unlocking the commercial potential for quantum computing.

In the development of its CryoIP product line, sureCore also used Siemens’s Analog FastSPICE platform and Siemens’ Solido™ Design Environment software, both of which demonstrated reliable and accurate operation at cryogenic temperatures, empowering sureCore to construct analog circuits, standard cell libraries, and memory designs including SRAM, register files, and ROM, using Semiwise’s cryogenic transistor models. Further, Siemens’ Analog FastSPICE software showcased exceptional capabilities in handling foundry device models at cryogenic conditions, helping deliver efficient analog, mixed-signal, and digital circuit design and verification functionality without convergence issues. The result is a high level of accuracy and performance, setting the stage for potentially groundbreaking advancements in quantum computing.

sureCore is rapidly progressing towards its first CryoIP tapeout, leveraging GlobalFoundries' 22FDX® PDK.

Paul Wells, CEO of sureCore, underscored the pivotal role of this partnership. "The critical storage element and the bit cell must essentially be treated as an analog circuit that is highly sensitive to process variability and mismatch,” said Wells. “When we develop new memory designs and their associated compilers, we need to run thousands of statistical circuit simulations to guarantee the yield and reliability of our IP. Our partnership with Siemens EDA has enabled us to leverage Siemens' Custom IC verification technology to build robust cryogenic IP cores, specifically tailored for Quantum applications."

"This partnership symbolizes Siemens' unwavering dedication to advancing the quantum computing domain,” said Amit Gupta, general manager and vice president of the Custom IC Verification Division, Siemens Digital Industries Software. “The groundbreaking technologies and solutions developed have the potential to redefine the boundaries of high-performance computing."

Siemens' Analog FastSPICE platform, powered by technology from Siemens’ Analog FastSPICE eXTreme™ platform, offers cutting-edge circuit verification for nanometer analog, radio frequency (RF), mixed-signal, memory, and custom digital circuits. It holds foundry certifications across all major foundries and is qualified across various process nodes, from mature to the most advanced. Siemens' Analog FastSPICE platform offers a comprehensive use model, including small signal, transient, RF, noise, aging, and multi-sim verification capabilities, with drop-in compatibility with industry-standard SPICE-based flows. This all-encompassing solution boasts high performance, capacity, and flexible features.

Siemens' Solido Design Environment plays a pivotal role by providing a comprehensive cockpit for nominal and variation-aware analysis and encompasses SPICE-level circuit simulation setup, measurements, regressions, waveforms, and statistical results analysis. Powered by AI technology, Solido Design Environment assists users in identifying optimization paths to improve circuit power, performance, and area - facilitating production-accurate statistical yield analysis, reducing runtime compared to brute-force methods.

Siemens Digital Industries Software pomáhá firmám všech velikostí s digitální transformací pomocí softwaru, hardwaru a služeb díky platformě Siemens Xcelerator. Software Siemens a komplexní digitální dvojče umožňují společnostem optimalizovat jejich konstrukční, inženýrské a výrobní procesy, aby se z dnešních nápadů staly udržitelné výrobky budoucnosti. Od čipů po celé systémy, od výrobku po procesy, napříč všemi průmyslovými odvětvími. Siemens Digital Industries Software – Accelerating transformation.

Note: A list of relevant Siemens trademarks can be found here. Other trademarks belong to their respective owners. sureCore, SureFIT and When low power is paramount are trademarks of sureCore Limited. Other trademarks belong to their respective owners

Kontakty pro tisk

Siemens Digital Industries Software PR Team
Email: yasmine.can@siemens.com