1. Home
Tisková zpráva

Siemens and AWS join forces to democratize generative AI in software development

8. ledna 2024
Las Vegas, Nevada, USA

Siemens and Amazon Web Services (AWS) are strengthening their partnership to make generative AI easily accessible to application developers across the Siemens Xcelerator ecosystem.
  • Siemens to integrate Amazon Bedrock into its Mendix low-code development platform to allow customers to create new and upgrade existing applications with the power of generative AI
  • Access to Amazon Bedrock’s advanced generative AI technologies will help customers accelerate digitalization and tackle skilled labor shortages
  • Mendix is an industry leader in low-code development with 50M end-users and more than 200,000 applications running on AWS across industrial, finance and other sectors

Siemens and Amazon Web Services (AWS) are strengthening their partnership and making it easier for businesses of all sizes and industries to build and scale generative artificial intelligence (AI) applications. Domain experts in fields such as engineering and manufacturing, as well as logistics, insurance or banking will be able to create new and upgrade existing applications with the most advanced generative AI technology. To make this possible, Siemens is integrating Amazon Bedrock - a service that offers a choice of high-performing foundation models from leading AI companies via a single API, along with security, privacy, and responsible AI capabilities - with Mendix, the leading low-code platform that is part of the Siemens Xcelerator portfolio.

“By integrating Amazon Bedrock into our low-code platform, we are democratizing generative AI technology and empowering everyone to create the applications customers need to become more competitive, resilient, and sustainable,” said Roland Busch, CEO of Siemens. “Making smarter applications without programming expertise accelerates innovation and helps companies to tackle skilled labor shortages.”

“Together, AWS and Siemens are empowering companies worldwide to create new capabilities, solutions, and value with generative AI,” said Adam Selipsky, AWS CEO. “This partnership builds on our 10-year relationship with Siemens, giving customers across all industries the flexible, customizable, secure environment they need to take advantage of new opportunities with generative AI.”

The combination will enable customers to select the generative AI model that best suits their specific use case and quickly and securely incorporate that model into their applications. This will make their development simpler, faster, and more efficient. Previously, when developers wanted to integrate generative AI models, they had to obtain access credentials, and write specialized function code. With the new Mendix-Amazon Bedrock integration, this can now be done with just a few clicks. Teams can create smart, industry-hardened applications without dedicated programming knowledge and users can interact with information easily via a graphical interface and the simplicity of a drag and drop commands.

This innovation allows Mendix customers to apply generative AI to drive productivity within their workforce. For instance, using generative AI, a factory worker can find machine documentation faster, generating relevant visualizations without a need to manually search a database, manuals, and records. A production engineer could also use generative AI to suggest machine adjustments to improve yield, and get suggestions on equipment adjustments, maintenance, or even spare parts to maximize a factory’s productivity. Customers do not need to build their own AI infrastructure and will be able to harness the power of their company’s data with the highest possible security and privacy, maintaining full control of their data.

Generative AI technology can supercharge applications with features like summarizing and analyzing lengthy technical or legal documents, translating content into different languages, or recognizing images. Financial businesses can integrate automatic fraud detection in their software, while workers in a car factory can improve quality based on AI analysis of millions of data points in the manufacturing line. With access to a choice of foundational models on Amazon Bedrock, users can easily select the best model for their specific task and integrate it with just a few clicks.

The collaboration expands on the long-established partnership between AWS and Siemens to help streamline the use of IT and cloud technology so it can be easily integrated in applications and machine workflows, making it seamless to engage with.

Today, more than 50 million end users worldwide work with more than 200,000 applications built with Mendix’s low-code platform, available as part of the Siemens Xcelerator portfolio. Low-code platforms are expected to grow substantially over the next years. The technology enables developers to create applications by drag and drop with reusable components and software building blocks, which means they can build more software faster and with smaller teams.

Amazon Bedrock is a fully managed service that offers easy access to a choice of industry-leading large language models and other foundation models from AI21 Labs, Amazon, Anthropic, Cohere, Meta, and Stability AI, along with a broad set of capabilities that customers need to build generative AI applications—simplifying development while supporting privacy and security. Users can also apply Guardrails to filter undesired content, adhere to responsible AI policies, or finetune their models using Knowledge Bases for Amazon Bedrock to give contextual information from private data sources and more relevant, accurate, and customized responses. The Mendix-Amazon Bedrock integration complements AWS’s other generative AI services, like Amazon CodeWhisperer, a machine learning (ML)–powered service that helps improve developer productivity by generating code recommendations based on developers’ comments in natural language and their code. Together, the services extend the benefits of generative AI to developers and enterprise users regardless of their programming abilities.

Siemens AG (Berlín a Mnichov) je technologická společnost zaměřená na průmysl, infrastrukturu, dopravu a zdravotnictví. Společnost vytváří účelné technologie, které zákazníkům přinášejí skutečnou hodnotu - od továren účinněji využívajících zdroje, přes odolné dodavatelské řetězce a inteligentnější budovy a sítě až po čistší a pohodlnější dopravu a pokročilou zdravotní péči. Spojením reálného a digitálního světa umožňuje Siemens svým zákazníkům transformovat jejich průmyslová odvětví a trhy a pomáhá jim tak měnit každodenní život miliard lidí. Siemens vlastní také většinový podíl ve veřejně obchodované společnosti Siemens Healthineers, předním světovém poskytovateli zdravotnických technologií, který utváří budoucnost zdravotní péče.

Ve fiskálním roce 2022, který skončil 30. září 2023, dosáhla skupina Siemens tržeb ve výši 77,8 miliardy eur a čistého zisku 8,5 miliardy eur. K 30. září 2023 měla společnost po celém světě přibližně 320 000 zaměstnanců. Další informace jsou k dispozici na internetové adrese www.siemens.com.